Creating a Hyperlink to a Logic Program

You can create hyperlinks to Logic programs such as ST Programs and Function Block Diagrams. This is useful on Mimics that show information that is related to the calculations and functionality that is provided by Logic programs.

To create a hyperlink to a Logic program:

  1. Display the Mimic that is to contain the new hyperlink. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Either:

    Or:

    Or:

    • Use the Animations feature to create a hyperlink (set the PickParam value to the address of the Logic program and enter the PickType value that corresponds to the type of hyperlink you require). For more information, including a list of PickType numbers, see Using Animations to Create a Hyperlink.
  3. Save the Mimic.

When the Mimic is displayed in Run Mode, selecting the 'trigger' object will cause the 'target' Logic program to be displayed in a new window or in place of the currently displayed Mimic (depending on the type of hyperlink you have configured).

If you want to link to the Form of a Logic program instead of the graphical display, see Creating a Hyperlink to a Form.


Disclaimer

ClearSCADA 2017 R2