Drag and Drop Menu Options for Values on Mimics

When you drag and drop a database item from the Database Bar onto a Mimic, a context sensitive menu is displayed. The options on the context sensitive menu vary according to the type of item you have selected.

The following list describes the possible menu options, but please be aware that some of the options are only available for certain items. For example, the Vertical Bar option is only available for analog points.

Further Information

Alarm Views: see Defining an Item or Group’s Alarm Properties in the ClearSCADA Guide to Core Configuration.

Help Views: see Specify a Help View in the ClearSCADA Guide to Core Configuration.

Alarm States: see Alarm Severity, Status, and Category in the ClearSCADA Guide to Alarms.

Default Views: see Defining a Default View in the ClearSCADA Guide to Core Configuration.

Schedules: see Using Schedules to Automate Regular Functions in the ClearSCADA Guide to Core Configuration.

Duty User: see Specify the Duty User in the ClearSCADA Guide to Alarm Redirection.

Data Grids: see Configuring Data Grids in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R2