Fill Animations

You can use the properties in the Fill group (on the Animations window) to animate the fill area of the Mimic object. The fill area is the inner part of a shape, text box, and so on.

You can animate the following Fill properties:

If you are animating the flash colors, the animations will only take effect if the Mimic object has the Blink property animated (or the Blink feature enabled on the object's Properties window, for example on a rectangle's Polyline Properties window).


Disclaimer

ClearSCADA 2017 R2