Edit a Pick Action Menu Option

You can change the settings for any of the custom pick action menu options. To make alterations, you need to display the Edit Action window.

To display the Edit Action window:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Double-click on the pick action that you want to edit. Alternatively, select the pick action and then select the Edit button.
    The Pick Action Configuration window is displayed.
  3. Use the Pick Action Configuration window to alter the configuration of the custom pick action (see Add a Custom Pick Action).

Disclaimer

ClearSCADA 2017 R2