General Tab (Embedded Trend)

The General tab contains Name, Visible, Animations, Pick Actions, ToolTip, and Dynamic Position settings that work in the same way as on other General tabs (see General Tab). However, the General tab on the Embedded Trend Properties window also contains some settings that are specific to embedded pre-configured Trends:

 

When you select the Background Color button, a color palette is displayed.

You can select any of the colors on the palette, or select the ... option to access the Color window. The colors on the palette are the system colors, and the Color window allows you to create a custom color (see Using the Color Window).


Disclaimer

ClearSCADA 2017 R2