General Tab (Embedded X-Y Plot)

The General tab contains Name, Visible, Animations, Pick Actions, ToolTip, and Dynamic Position settings that work in the same way as on other General tabs (see General Tab). However, the General tab on the Embedded X-Y Plot Properties window also contains some settings that are specific to embedded X-Y Plots:


Disclaimer

ClearSCADA 2017 R2