Mimic Properties Window

Each Mimic has a Mimic Properties window that you can use to define the default settings for:

The way in which you display the Mimic Properties window determines whether the changes apply to a specific Mimic or every Mimic on your client:

The default settings that you define on the Mimic Properties window are used for new objects that you add to a Mimic (regardless of the means by which you access the Mimic Properties window). For example, if you specify Text Font settings on the Mimic Properties window, any text boxes that you add will use those settings by default.

The Mimic Properties window consists of several tabs, each containing a variety of settings. You can use the tabs as follows:

Some Mimic options can only be configured on a per-Mimic basis, including the Layers, Views, and Script settings.

The default settings that you specify using the Mimic Properties window are just a starting point - each object that you add to a Mimic also has its own properties window. You can use the individual Mimic object properties windows to configure each Mimic object as required. For details about the properties windows for individual Mimic objects, see Editing Objects on a Mimic.


Disclaimer

ClearSCADA 2017 R2