Simple Modbus Channel Status Attributes

These status attributes are specific to channels on the Simple Modbus driver:

Two further status attributes, Primary Eavesdrop Tx Assign, and Secondary Eavesdrop Tx Assign are not used by the Simple Modbus driver.


Disclaimer

ClearSCADA 2017 R2