Configuring String Points

Use OPC XML-DA String Points to map text strings on OPC XML-DA servers into ClearSCADA.

Configure the properties of each String point using the fields on the OPC XML-DA String Point Form.

For information the String Point tab on the String Point Form, see Defining String Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on the OPC XML-DA tab, see Configure Common Point Properties on the OPC XML-DA Tab.

For information on the Control tab, see Define the Control Settings for a String Point in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R2