Differences Between the WebX Client and ViewX

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of ClearSCADA. For information about the WebX client that is supported by ClearSCADA 2015 R1 onwards, for which the web server is hosted using IIS, click here.

Many of the functions and displays that are available from a ViewX client are also available from a WebX client—see the other sections of this guide for more detail:

The differences in how you use a WebX client compared with ViewX mostly relate to how you access items and functions.

The main differences between a WebX client and ViewX are:

Further Information

Run a WebX Client.


Disclaimer

ClearSCADA 2017 R2