Pager Specific Alarm and Event Categories

Each alarm and event on a ClearSCADA system has a Category that indicates the type of alarm or event. The Category is included in the Events List by default and, if applicable, is also included in the Alarms List and the Alarm Banner.

If required, you can filter the entries in the Events List or Alarms List by category. You can choose to filter the lists by a variety of ‘core’ categories as well as any categories that are specific to the drivers that are installed on your system.

On systems that have the Pager driver components installed, the ‘core’ alarm and event categories are available as well as these Pager-specific categories:

Further Information

Filter Categories: see Filter a List in the ClearSCADA Guide to Alarms.

Alarm Banner: see Alarm Banner in the ClearSCADA Guide to Alarms.

Alarms Lists: see Alarms Lists in the ClearSCADA Guide to Alarms.

Events List: see Events Lists in the ClearSCADA Guide to Lists.


Disclaimer

ClearSCADA 2017 R2