SCADAPack x70

Define the Modbus Slave Device

When you create a Modbus Point Scanner you need to associate it with a Modbus Slave Device configuration item.

Modbus Slave Device

This allows you to select the Modbus Slave Device that the point scanner is associated with.

Use the browse button to display a Reference browse window and then select the required entry from the window.


Disclaimer

ClearSCADA 2017 R2