Mimic Properties

Mimic Objects have properties associated with them. For more information on these properties, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

NOTE: The Mimic.Layers property provides access to the animation properties of any Mimic item. For many Mimic items, these properties correspond to the entries for that item on the Animation window, but there are a few exceptions—see Animation Properties for Mimic Items on Layers.

Mimic Object also have the following Control Object properties which are normally associated with the Control Objects returned by Form functions and properties:


Disclaimer

ClearSCADA 2017 R2