Disable External Authentication

You can disable External Authentication on your system at any time by clearing the Enabled check box in the External Authentication section. When you disable External Authentication, every aspect of ClearSCADA user account management has to be undertaken within ClearSCADA.

To disable External Authentication:

  1. Display the Server Configuration Tool and log on if required.
  2. Expand the System Configuration branch.
  3. Select the External Authentication entry.
  4. Clear the Enabled check box.

  5. Apply the changes to the server.
    Any user accounts that were configured to be authenticated via Windows or LDAP will now require a password to be set in ClearSCADA. Without a ClearSCADA password, a user will be unable to log on via the account. Likewise, any ClearSCADA user accounts that were created automatically as a result of the Create Users Automatically from Group Membership option being selected will also require a password to be set in ClearSCADA to enable those accounts to be used.

Further Information

Define the Password for a User

Setting Up Security for WebX and Original WebX Clients.


Disclaimer

ClearSCADA 2017 R2