Status Attributes Associated with User Accounts

Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Use this section if you need information about the status of a user on the system.

This section summarizes the status attributes that are specific to User Accounts. The status attributes comprise:

The Date Format setting on the user's account defines the format used for the date and time entries in the Status display (see Define the Regional Settings for a User).

Further Information

View information about multiple User Accounts: see the Users List.


Disclaimer

ClearSCADA 2017 R2