User Accounts for Third Party Applications

Third Party applications such as OPC client applications also access the ClearSCADA system via a user account. The type of access that is permitted for Third Party applications is dependent on whether the Third Party application supports client security:

Further Information

Configuring the Guest User Account

Creating a User Account.


Disclaimer

ClearSCADA 2017 R2