View the Status of Database Backups

The amount of time it takes to make a backup of your database will vary, depending on the amount of data you are backing up. As the backup progresses, ClearSCADA logs several events, such as:

 

During a backup, the 'action' event messages (Backup Requested and Backup Request Successful) are displayed in the Status Bar at the appropriate stage of the backup process.

Backup event shown in status bar

If a Backup is unsuccessful, an alarm is raised. The alarm is shown on various Alarm displays, including the Alarm Banner and Alarms List.

You can also view the current status of a backup by:


Disclaimer

ClearSCADA 2017 R2