DA Items

The DA Items category provides status information about each OPC DA tag to which an OPC DA client is subscribed. Status information for OPC DA tags is shown when OPC is used to access the database. Each OPC DA tag represents a path to a value.

The status information for each OPC tag is categorized as:

You can use the DA Items status information to investigate Mimic Update Problems.


Disclaimer

ClearSCADA 2017 R2