Interest

The Interest category provides status information about each database interest reference that is currently made between the server and the client(s). A database interest reference is made each time the server sends data to a client.

Each entry in the Interest category represents one interest reference i.e. one set of data that has been sent from the server to the client(s).

The status information is categorized as:


Disclaimer

ClearSCADA 2017 R2