Links (Server)

The Server Links category provides status information about each link from a client to the server.

ClearSCADA requires multiple links, with the number of links varying depending on the size of the system. In many cases, the number of links that each ViewX client uses is approximately:

The status information for the links is categorized as:

You should pay particular attention to the number of links in the Server Links category—there should not be an excessive number of links in comparison with the number of clients. You should also check that the Longest Req is generally less than 1000mS.

An excessive number of links or a Longest Req over 1000mS may indicate a high server load, see Diagnose Client Performance Problems.


Disclaimer

ClearSCADA 2017 R2