Links (WebX)

The WebX branch of the Server Status Tool includes a Links category. The Links category in the WebX folder on the Server Status Tool provides status information for the connections between the server and any WebX clients.

The status information for the WebX links is categorized as:

You should pay particular attention to the number of links shown in the Links category, and the Long Time status value.

If the number of links is excessively high in comparison to the number of WebX clients (typically, there are between 1 and 3 links per WebX client), you should contact Schneider Electric for assistance.

If the Long Time status value is more than 1000mS, there may be a high server load (see WebX Client Activity).

Further Information

WebX Status Information.


Disclaimer

ClearSCADA 2017 R2