WebX Status Information

The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The WebX group provides status information about any WebX clients that are connected to the server and the cookies, links and threads that they use. The WebX group contains the following sub-categories:

Further Information

WebX: see WebX Client

Is WebX activity causing a high load on the server? see WebX Client Activity.

Database Web Server Connection Problems.


Disclaimer

ClearSCADA 2017 R2