System Analysis

This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the ClearSCADA system. This section applies to most simple drivers. For driver-specific information, see the individual driver guides. For more general information on analyzing a ClearSCADA system, see System Analysis in the ClearSCADA Guide to the Server Status Tool.

During system analysis, you might need to:

Additionally, if a scanner is not communicating with the server when it should be, see Troubleshooting.

When troubleshooting on a ClearSCADA system, always check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that ClearSCADA has detected.


Disclaimer

ClearSCADA 2017 R2