Unlock

Associated with: Sofrel output points

Security permission required to access this option: Control

This pick action is only available when used in conjunction with outstations that use the LACBUS-RTU protocol.

An output point in a Sofrel outstation may be locked to prevent it from being controlled by the outstation's process control programs. Unlocking a point allows it to controlled from anywhere, including by process control programs.

The Unlock pick action is available on a point providing that:

Select this pick action to unlock the point.


Disclaimer

ClearSCADA 2017 R2