Example Projects Overview

The Example Projects database has been designed to help you understand the concepts and benefits of ClearSCADA. When you logon for the first time using any of the three User Accounts provided in the database you automatically see the Opening Page. The Opening Page is a Mimic and is part of the Example Projects database, it is also referred to as the Home Page.

This page provides you with three options:

Presentation

This option allows you to view a comprehensive and interactive presentation of the key features of ClearSCADA.

Projects

This option allows you to view a typical project and observe how the various interactive functions of ClearSCADA can be applied within a project environment.

This is an interactive set of Mimics that allow you to explore an example set of projects that illustrate how a project can be constructed.

You can also find more detailed information in the ClearSCADA online help (see Display ClearSCADA Help).

What's New

This option allows you to review the new features in the current version of ClearSCADA.

Further Information

Welcome to the ClearSCADA Tutorial


Disclaimer

ClearSCADA 2017 R2