Define the TBox Properties

Use the fields on the TBox tab of the relevant TBox Outstation Form to configure these properties:

The first three fields on the TBox tab are used to uniquely identify the TBox device. A TBox RTU can be addressed by a combination of Address, Sub Address, and Station Name. Use whichever combination of these fields are required for your system's addressing scheme.


Disclaimer

ClearSCADA 2017 R2