Retrieve Historic Data

Associated with: TBox outstations

Security permission required to access this pick action: Retrieve Data

ClearSCADA retrieves historic data at the frequency specified on the Outstation Form (see Define the TBox Properties). Use the Retrieve Historic Data pick action to retrieve historic data between the scheduled intervals. Historic data consists of Chronologies and Sampling Tables from the TBox RTU.

Select the pick action to display the Retrieve Historic Data window.

Use the Historic Data Retrieval Mode combo box to specify the data to be retrieved:


Disclaimer

ClearSCADA 2017 R2