System Analysis
This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the ClearSCADA system. This section applies specifically to the TBox driver. For more general information on analyzing a ClearSCADA system, see System Analysis in the ClearSCADA Guide to the Server Status Tool.
During system analysis, you might need to:
Additionally, if an RTU is not communicating with the server when it should be, see Troubleshooting in the ClearSCADA Guide to Advanced Drivers.
When troubleshooting on a ClearSCADA system, check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that ClearSCADA has detected.