Locate in OPC Data Explorer
This option is only available if:
- You are accessing an Object menu from ViewX (other than from the OPC Data Bar)
- Your user account provides access to the OPC Data Bar.
Select the Locate in OPC Data Explorer option for ClearSCADA to display the OPC Data Bar and highlight the item in the hierarchical ‘tree’ structure within that Explorer Bar.
Also see Locate in Database Explorer.
You can also locate an item in the OPC Data Bar by using the Locate command on the ViewX ribbon (see Display an Explorer Bar in ViewX).