Locate in Database Explorer

This option is only available if:

Select the Locate in Database Explorer option for ClearSCADA to display the Database Bar and highlight the item in the hierarchical ‘tree’ structure within that Explorer Bar.

Also see Locate in OPC Data Explorer.

You can also locate an item in the Database Bar by:


Disclaimer

ClearSCADA 2017 R2