Understand the WebX Interface

When you log on to a WebXclient, the interface includes a combination of the following components:

The Alarm Banner informs you about the current alarm activity on the system You navigate the system using the navigation bar and the Explorer Bar. You view the displays and information you require in the document display area (in some cases, you use the object-specific options to perform further activities or access other displays). The Status Bar provides information relating to user activity.

For more information about these components, see the following sections:

Further Information

Understand the ViewX window.


Disclaimer

ClearSCADA 2017 R2