Device Ports for WITS Field Devices

When you are configuring a connection between a WITS Field Device and ClearSCADA, you will need to specify a Device Port. The Device Port is a physical or logical communications port on the Field Device. You can find the Device Port settings on the Direct, PSTN and Network tabs on the Outstation Form (see Display a Form).

When you configure the Device Port settings in ClearSCADA, you need to choose the communications port that the Field Device uses for the connection you are configuring. For example, if you are configuring a network connection between ClearSCADA and the E1 port on a Schneider Electric Talus T4e Field Device, you would set the Device Port to Ethernet 1 (Outstation Form >Network tab).

The options that are available to select in the Device Port settings are taken from the Device Profile for your Field Device (see WITS Device Profiles).

To specify the Device Port for a connection, you need to use the Outstation Form. There are Device Port settings for:


Disclaimer

ClearSCADA 2017 R2