WITS Configuration Strategies

There are many different configuration strategies you can use to configure your WITS Field Devices for the first time. The strategy that you choose to use will depend on the capabilities of your Field Device and its Configuration Application, the quality of the communications infrastructure, and other factors such as whether you want to use ClearSCADA's Group Templates feature. These are explained in detail in Choosing a Configuration Strategy for WITS.

Before you choose a WITS configuration strategy, you need to be aware of the general process for configuring a Field Device, and the tasks that are common to several different strategies. The common tasks of the configuration process include:

The order in which you need to perform these tasks will vary depending on the strategy you choose. For some strategies, you will need to perform all of the tasks, whereas for others you will only need to perform some of the tasks.

If you are unsure which strategy is most appropriate to your requirements, see Choosing a Configuration Strategy for WITS.

To make configuration changes to WITS Field Devices that have already been set up to work with ClearSCADA, see Making Changes to WITS Field Device Configuration

Further Information

Pre-Requisite ClearSCADA Configuration for WITS Field Devices

Configure Most Settings using the Configuration Application

Configure Most Settings using ClearSCADA

Pre-Configure ClearSCADA - Upload or Import Later

Using Group Templates with WITS Field Devices


Disclaimer

ClearSCADA 2017 R2