Automation Interface Methods

In addition to the pick actions that are available in ViewX, additional methods (pick actions) are available using the ClearSCADA Automation Interface.

The topics in this section provide information about methods that are specific to the Wonderware Historian driver.

The following method is available on Wonderware Historian database items when using the Automation Interface:

To find out about the methods that are available for each type of database item, please refer to the Database Schema (see Working with the Database Schema). The Database Schema provides details on the name and arguments of each method, so that you can call the methods from your own programs and scripts.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2