Specify the HCAL Store-and-Forward Cache Properties

Use the fields within the Store/Forward section of the Wonderware Historian tab to specify the properties of the HCAL store-and-forward cache. HCAL uses this cache to temporarily store export data if the network connection to the Wonderware Historian is unavailable or intermittent. Once the link becomes stable or available again, HCAL will forward the cached data to the Wonderware Historian.

Further Information

Specify a Folder for the HCAL Store-and-Forward Cache

Wonderware Historian documentation.


Disclaimer

ClearSCADA 2017 R2