Configure an Advanced OPC Group

An Advanced OPC Group is a logical grouping of points that the Advanced OPC DA Driver retrieves data from at the same interval.

You can attach multiple Advanced OPC Groups to one or more Advanced OPC Server on your system. Each group can have different update rates, deadbands and keep alive intervals (these are all asynchronous settings).

If you are using OPC DA 3.0 you can have per point deadbands.

Configure the Group’s properties using the Advanced OPC Group Form. Use the fields on the Group tab to define the driver-specific properties of the group:

Properties on other tabs are common to many database items, see Tabs That are Common to Many Configuration Forms in the ClearSCADAGuide to Simple Drivers.

For information on the minimal amount of configuration that you can undertake to produce a functional Advanced OPC Group in ClearSCADA, see Minimum Configuration.


Disclaimer

ClearSCADA 2017 R3