Managing ClearSCADA Alarms in Wonderware InTouch

You can view and manage ClearSCADA alarms from within Wonderware InTouch. To do this, you need to install the ClearSCADA Wonderware Alarm Provider component (see Wonderware Alarm Provider Component) and you need to enable the Wonderware Alarm Provider driver using the Server Configuration Tool.

The ClearSCADA component supports redundancy and disconnection from the Wonderware InTouch alarm system with no data loss. You will need to do some configuration within Wonderware InTouch (see Configure Wonderware InTouch to Access Database Alarms).

In addition, you will also need to know How ClearSCADA Alarm Fields are Mapped to Wonderware InTouch Alarm Fields.


Disclaimer

ClearSCADA 2017 R3