Install the Wonderware Alarm Provider Component

If you want to view and manage ClearSCADA alarms from within Wonderware InTouch, you need to install the ClearSCADA Wonderware Alarm Provider component and you need to enable the Wonderware Alarm Provider driver using the Server Configuration Tool. You can do this when you first install ClearSCADA (see Installing ClearSCADA) or you can modify your existing installation (see Making Changes to your ClearSCADA Installation). You can find the Wonderware Alarm Provider component in the Server section of the Custom Setup page of the ClearSCADA Installer Wizard.

When you perform a Full or Typical ClearSCADA installation, the ClearSCADA installer does not automatically install the Wonderware Alarm Provider component. You need to do a Custom installation and manually select the component.


Disclaimer

ClearSCADA 2017 R3