Installing ClearSCADA

You can install ClearSCADA on any server or client computer that meets the recommended specifications:

You can use the ClearSCADA DVD to install ClearSCADA server, ClearSCADA Client, and Data Access components. You will choose which components are to be installed during the installation process.

To install ClearSCADA on a server or client computer:

  1. Run the ClearSCADA Installer and select the Install ClearSCADA option.

    The Installer will then either:

    • Run the ClearSCADA Setup Wizard. The Setup Wizard provides a series of ‘pages’ that guide you through the installation process.

    Or:

    • Install any prerequisite software that is not already installed on your computer. The software is installed from the ClearSCADA DVD. When the prerequisite software is installed, the Setup Wizard will run.
  2. Use the various ‘pages’ of the Setup Wizard to make selections relating to the ClearSCADA installation:

Further Information

Prerequisite Components

ClearSCADA System Requirements.


Disclaimer

ClearSCADA 2017 R3