Configuring Analog Points

The Hilscher driver supports Analog Input and Analog Output points.

Configure the properties for each analog point using the appropriate Point Form. Choose from:

This section covers configuration of properties on the Hilscher tab of each Form. Use the Hilscher tab to:

For information on the Analog Point tab, see Defining Analog Point Details in the ClearSCADA Guide to Core Point Configuration.

If the point is an output point, you also need to enable and configure the properties on the Control tab—for information, see Define the Control Settings for an Analog Output Point in the ClearSCADA Guide to Core Point Configuration. Optionally, you can also use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration).

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3