Tabs on Point Forms

Point Forms have several ‘tabs’ or ‘pages’ for configuring different aspects of point data. For many points on simple drivers, these tabs are available:

In addition, on drivers that support controls (outputs), a Control tab and a Control Checks tab are displayed.

For information on configuring the properties on the Control tab, see the driver-specific documentation for any driver-specific fields, and also, as appropriate:

For information on configuring the properties on the Control Checks tab, see Configuring Control Checks Settings in the ClearSCADA Guide to Core Point Configuration.


Disclaimer

ClearSCADA 2017 R3