Control with Qualifier

Associated with: IEC 60870-5 Digital Output Points

Security permission required to access this pick action: Control

The type of control that an IEC 60870-5 digital output point supports differs, depending on the type(s) of control that are supported by the outstation on which that point resides.

Use the Control with Qualifier pick action to control an IEC 60870-5 digital output point. Select the pick action to display the Control with Qualifier window. Use the fields in the window to specify the control that ClearSCADA is to perform:


Disclaimer

ClearSCADA 2017 R3