Define the Severity of Lufkin SAMS Controller Events

ClearSCADA assigns a severity level to the Lufkin SAMS controller events that it stores in the database. Use the Event Severity combo box on the Lufkin SAMS tab to specify the severity level that ClearSCADA assigns to those events.


For more information about severity levels, see Defining Severities in the ClearSCADA Guide to Core Configuration.

You use the Upload Event Log pick action to upload a controller’s events to ClearSCADA (see Actions that are Specific to the Lufkin SAMS Driver).


Disclaimer

ClearSCADA 2017 R3