Upload Event Log

Associated with: Lufkin SAMS controllers

Security permission required to access this pick action: Retrieve Data

Use the Upload Event Log pick action to upload to ClearSCADA the entries that are stored in the controller’s Event Log. The pick action enables ClearSCADA to upload multiple events at a time, should more than one event exist in the controller’s Event Log at the time that the pick action is triggered. ClearSCADA stores the controller’s events in the Event Journal. Each controller event:

The controller’s Last Outstation Event status attribute provides information about the latest controller event that ClearSCADA has uploaded (see Lufkin SAMS Controller Status Attributes).

NOTE: If using this pick action with the Automation Interface, you need to specify the method name UploadEventLog.


Disclaimer

ClearSCADA 2017 R3