Last Outstation Event

Associated with: Lufkin SAMS controllers

This status attribute displays information about the latest controller event to be uploaded to ClearSCADA. The information includes:

The status attribute is displayed once ClearSCADA has retrieved an event from the controller’s Event Log (see Upload Event Log).The status attribute provides information about the controller event that has the latest time stamp in the collection of controller events that ClearSCADA last uploaded. (For information about earlier controller events, see the Events List.)

Example:

Id: 27, Description: "Gauge Off Time Changed", occurred at 25/Jul/2012 11:42:45.000


Disclaimer

ClearSCADA 2017 R3