Editing a View

To change the positioning or magnification of an existing View:

  1. Display the Mimic that contains the View you want to edit. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Select Views in the View command group on the Graphics Tab.

    The Views window is displayed.

  3. Select the View you want to edit from the Views list, then select the Properties button.
    The Edit View window is displayed.

  4. Overwrite the Name entry as required.
  5. Change the Position of the View by altering the coordinates in the X and Y fields. X is the positioning from left to right and Y is the positioning from top to bottom.
  6. Change the level of magnification (Size) by altering the W and H settings. W is the width setting and H is the Height setting. Increasing the numbers reduces the level of magnification; reducing the numbers increases the level of magnification.
  7. Select the OK button to confirm the settings and close the Edit View window.

Alternatively, you may find it easier to create a new View with the required settings then remove the existing View (see Removing a View).

Only users with the Configure permission can edit Views.


Disclaimer

ClearSCADA 2017 R3