Configuring Digital Points

The Mitsubishi driver supports multi-bit Digital Input and Digital Output points.

Configure the properties for each digital point using the fields on the Mitsubishi Digital Point Form.

This section covers configuration of properties on the Mitsubishi tab of the Form. Use the Mitsubishi tab to Configure the Mitsubishi Point Properties.

For information on the fields on the Digital Point tab, see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3