Configuring a Mitsubishi Channel

A Mitsubishi Channel provides ClearSCADA with additional connection information so that the server can communicate successfully with Mitsubishi PLCs and Mitsubishi Slaves.

Specify the properties for a channel using the fields on the Mitsubishi Channel Form.

The Form has several tabs (see Tabs That are Common to Many Configuration Forms in the ClearSCADA Guide to Simple Drivers).

Use the Channel tab to Configure the Basic Channel Properties.

Mitsubishi Channels use RS-232/RS-485 serial communications. Use the fields on the Connection tab of the Form to specify the required properties for a channel’s serial connection (see Configure a Channel’s Serial Connection Properties in the ClearSCADA Guide to Drivers).

For fields on the other tabs, see Tabs That are Common to Many Configuration Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3