Configuring a Simple Modbus Scanner

A Simple Modbus Scanner is logical functionality that runs within ClearSCADA and scans for data on a Modbus PLC or a Modbus Slave.

Configure a scanner for:

We recommend that you configure separate scanners to scan different blocks of registers in a range, if those blocks are some distance apart. This is more efficient than having one scanner scan a large range that includes many unused registers.

You can configure a Scanner’s properties using the fields on the Simple Modbus Scanner Form. The Form has several tabs:

For information on the minimal amount of configuration that you can undertake to produce a functional Simple Modbus Scanner in ClearSCADA, see Minimum Configuration.

For examples showing how to configure a scanner to fulfill Modbus scanning requirements, see Configuration Examples.


Disclaimer

ClearSCADA 2017 R3