Comms Statistics

Associated with: OPC XML-DA scanners

This attribute indicates the number of:

since the scanner was last restarted.

Example:

42 reads, 30 read items, 12 writes, 0 connection closes

Use the Error Statistics attribute to ascertain whether any of the read or write operations listed above generated errors.


Disclaimer

ClearSCADA 2017 R3